Hello,
I configure my OMAP EVM3530 to have USBFn RNDIS as Boot Device and Debug Device. After power-on, I got the output shown below on the UART3 terminal. A window is also poped up asking to install a USB driver "Microsoft RNDIS KITL for OMAP2430".
Would you please show me Where I can get this driver? I did install the USB driver that goes with EVMFlash tool and able to download the XLDR to the EVM through USB but I think this must be another one. I do not know which version of BSP from BSquare that I am using. It must be 6.11 or 6.12. Do I need to install 6.14 for RNDIS to work?
I appreciate your help.
Luan
Hit space to enter configuration menu 5...
Hit space to enter configuration menu 4...
Hit space to enter configuration menu 3...
Hit space to enter configuration menu 2...
Hit space to enter configuration menu 1...
HostMiniInit:: !!
Rndis:: initialization: with addr=480AB000
Rndis:: Address static map to addr=480AB000
Rndis:: initialization!
+USBFN::Device ID = 0x4b7ae02f
+USBFN::Device ID = 0x4b7ae02f
Rndis:: PDDInit Success!
Rndis:: Get MAC address 200,902F,B5D
Rndis:: initialization: Fail!
ERROR: Boot device driver Init call failed