I'd like to confirm following points. Could anyone can answer them?
1) What's the conditions of whether it displays custom option or not? Where can we check it via API?
2) Can we just ignore the condition of the website when the option is displayed ? I mean, In Order API, there is option called CustomReel. Can we just make it true if needed? Is there any conditional constraint for customreel to be enabled?
3) I've heard that you have to setup module to enable CustomReel option. Where do we setup module? Is there any instruction document for that?