This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-API: API 2.0 _ Payment information setting in production environment

Hi Paul, 

We met the same error in the production environment.

Please help pass to the account manager to adjust the setting for the nine ID!

Thanks!

Error: Check your line of credit information and provide the correct information and resubmit the request. For additional information refer to api-portal.ti.com/order-api-payment

1. FC*6B
2. FB*15
3. FC*5A
4. FC*B4
5. FB*8B
6. FC*26
7. FC*DD
8. FC*DD
9. FD*4D

**Attention** This is a public forum