This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5450:TPS5450DDA

Part Number: TPS5450

Tool/software:

IC "No output "the input DC is powered on.

The pad is 24V to 12V.

When the input is powered on at 24V, the output voltage cannot rise to 12V normally, and the current does not reach the Current Limit. Why does the IC enter the hiccup state?

Please tell the reason is and how to solve it.

**Attention** This is a public forum