This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUCK-CONVCALC: Converter

Part Number: BUCK-CONVCALC

Tool/software:

Hi,

We are looking for DC-DC converter with specification as follows:

Input Voltage : 18V - 75V

Output Voltage: 5V/1.2A = 6W Isolated output

Isolation of 4 - 6kV between input & output.

Request you to suggest suitable converter module to incorporate in our design.

**Attention** This is a public forum