This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-API: BackLog API Create Order/Quote Connected Failed

Part Number: TI-API

Tool/software:

transact.ti.com

API Address ; v2/backlog/orders/test

When I use the  Post method  to create Backlog Test Order  ,

the Response Return Connected Failed,

This solution start  from 2-3 days ago, I can't create the  backlog order , or backlog quote order

But ,I can create store order with my program.

By the way , I  also can retire the  backlog order detail which created previously.

I don't know it a  network error , or a  program error 

My Network location is  China , Nanjing

{"order":{

"checkoutProfileId":"my checkoutProfileId",

"customerPurchaseOrderNumber":"TI_2025060509_4999",

"purchaseOrderDate":"2025-06-05","endCustomerCompanyName":"My CompanyName ","lineItems":[{"customerLineItemNumber":"101271","tiPartNumber":"SN74HC00DR","customerPartNumber":"SN74HC00DR","customerAnticipatedUnitPrice":0.048,"quoteNumber":"26936530","customerCurrencyCode":"USD","schedules":[{"requestedQuantity":7500,"requestedDeliveryDate":"2025-06-05"}]}]}}

**Attention** This is a public forum