This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L21EVM-PDK: Controlling the ADC from another Windows application

Part Number: ADS127L21EVM-PDK
Other Parts Discussed in Thread: ADS127L21

Tool/software:

Dear support,

We are going to use ADS127L21 in our ongoing project. The fastest option for our application is to use the "TI hardware"  (Eval board +  PHI EVM controller) and to be able to control the ADC from our Windows application. I'm aware of the provided embedded driver source code in C (which is in this setup running on the PHI EVM controller).

 Are you by any chance able to provide us (1)a Windows dll (precompiled + possibly the source) which we can load into our Windows application and control the ADC, and (2)the accompanying firmware for the PHI EVM controller? You can likely create such a dll by stripping down the existing Windows Demo application. 

Thank you,
Kind regards,
Zoran

**Attention** This is a public forum