Other Parts Discussed in Thread: INA199, LM5156, PMP10081
Tool/software:
Hi, I am working on a concept to make a constant current flyback converter.
My idea:
Use INA199 to sense the current from an Rsense connected in series with the output secondary winding and connect the output of INA to the FB pin of LM5156. Rsense is calculated based on gain of INA(50V/V) and the current that i want to control.
Problem:
Somehow the converter is not working based on current feedback. The circuit is always working on OCP protection now. FB value stays at 700mV approx.
Questions:
Does this concept makes sense?
Can INA199 source current to the PWM controller?
Any valuable suggestions are highly appreciated