This thread has been locked.

TMUX1308-Q1: TMUX1308-Q1

Part Number: TMUX1308-Q1


Tool/software:

I would like to select between two signals to pass from input to output (low current <50 mA ).  electromechanical relay is a solution as I know normally closed (NC) and normally opened (NO) states.  However, electromechanical relays have lower reliability.  for Tmux1308-Q1 what is the state if the 5V supply is lost? 

2- I appreciate a potential solution using either a MUX or solid state relay

**Attention** This is a public forum