This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
We are in the process of setting up the Integration between Our SAP application with your TI system
Port is the gateway through which data comes into or goes out from a system. Every RFC destination, or in other words, every system would have a port no. assigned to it, which would also already be maintained.
Kindly please provide the Port no./Service no. to connect the target system (TI system).
Regards
Shameer
Hi Shameer,
Below is a list of our web proxy firewall ports. ,Please remember that your myTI credentials (and key/secret) are required in order to successfully test.
Also know that, myTI customers with a myti company account that have requested access to receive push notifications from (HTTP POST requests from ticom-webservice app servers, may need to open your company firewall ports to allow access for the listed IP addresses to receive the push notifications.
PLEASE NOTE: The Web Proxy Server IP addresses listed below can be used at any time. TI does not restrict or limit to a single API in a single region.
Dallas
192.91.75.29
192.91.75.30
192.91.75.12
192.228.67.12
192.228.67.13
192.228.67.14
California
192.153.236.16
192.153.236.17
Europe
192.91.60.14
192.91.60.15
Hong Kong
192.163.20.231
192.163.20.232
Singapore
192.163.15.6
192.163.15.7
India
192.163.5.9
192.163.5.10
Japan
192.91.109.11
192.91.109.12
**Attention** This is a public forum