This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have got TI product information ,there are some questions:
1.TPD4S010DQAR (:ESD & surge protection ICs), information from TI website, Length of this part is "2.5mm",but API feed back this is "2"
SN74AUP1G32DPWR (:OR gates) API feed back Length , width ,pin pitch , MaxHeight are all "0".
2. We can get product parameter value, but we don't know parameter's unit ? Can you share TI 114 commodities parameters' unit.
3. What's the definition of "automotive qualified" ? Is it refer to temperature range is -40°C-+125°C? or is this part AECQ qualified?
4.Can we get device image,symbol and footprint,fab,
5. Can we get part fab, assembly site information?
Hello
no we do not provide the information requested from item 4 and 5 above in our product API -
I will have to talk to our product lines to find out some of the information or direct you to whom may can answer these questions. let me come back to you tomorrow with more information.
For some of these technical questions if you go to the Power Management forum - they should be able to assist with the technical questions.-this is their forum - (+) TI E2E support forums and additionally when you executed the product API the link in your json response takes you to the product page that also once on the ti.com product page leads you to more information of that product such as the datasheet, and additional info.
Hello Liu,
I understand you may still need some information as I did not quite answer all of your questions. - our technical product support has provided a little more insight to your questions that you have asked - pleas allow me to address these Questions below
Question 1 and 2 I am in contact with technical team on these 2 issues you have shared - they are actively looking into the issue you have reported.
Question 3- automotive qualified -- please see the definitions on this page: https://www.ti.com/support-quality/certifications-and-standards/part-ratings.html For automotive, Designed for automotive applications, automotive-classified parts help designers meet Automotive Electronics Council (AEC)-Q100 or AEC-Q101 standards, or other automotive specifications. See the product’s data sheet for details.
Question 4 and 5, we do not provide this information or data within the API, but allow me to direct you to Ti.com to assist with your request example https://www.ti.com/product/OPA333#cad-cae-symbols and regarding available material attributes this page https://www.ti.com/material-attributes-search/
As the technical team shares updates for Issue 1 and 2, I will respond back to you at that time.
Question 1 and 2 technical team Q1 we need a little more info. on Q2.
Would you be willing to pull the data again and share back what you may be receiving in your response, to see if we have corrected or still may be missing details you are requesting.
1.TPD4S010DQAR:Length has been correct,but there's not any unit for these parameter values.
2.SN74AUP1G32DPWR:Width and Length have been correct without parameter unit, but Pitch、MaxHeight remained "0".
Thank you, I have shared the information back to the tech team so they can review...
The units should be mm, i do not see that we display it but it is in the spec as such, that height, length, pitch and width are mm.
I know the length , width unit is mm, but there are other parameters we need to know the unit ,for example, voltage, current etc.
**Attention** This is a public forum