Tool/software:
Hi all,
This is kihwan lee from korea.
I'm trying to run example Running Application in AUDIO-SDK--FREERTOS-AM275-AWE_10.01.09.
My environment is windows.
I think I succeed below two example Running application as below .
Llke these :
But I think I failed to run config 3.
I think it's because wrong setting below "BUILD_AWE_MULTI=1"
Is it right to set as below in command window. ?