Part Number: DP83869-EP
Other Parts Discussed in Thread: DP83869
Hi Team,
I have a customer testing ethernet compliance 1G on the AM64x EVM. They have the same implementation on their custom board and seeing similar failures.
There are some failures observed. Please refer attached. Could you please provide some suggestions for improvement. Any registers that can be programmed.
Could we change the Rbias 11K to 10K for the DP83869.
Is there a compliance report for DP83869 that could be shared with customer.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1036/8611.AM64_5F00_EVM_5F00_002.mht
Additional customer questions
Thanks for https://www.ti.com/lit/an/snla239b/snla239b.pdf ; there is some very interesting feature related to DP83687 :
It seems that this register is related to PROG_GAIN MDI, which have been removed from DP83687 datasheet, and not present into DP83869’ one.

Is it a kind of hidden register inside DP83869 ? which should be set for Test Mode 1 (even un-documented)?
Additional question
Do you use separate Magnetic + RJ45 on the brick or do you have them integrated like the AM64x EVM
On our board we’ve got the same architecture than AM64 EVM GP (RJ45 embed Magnetic).
for https://www.ti.com/lit/an/snla239b/snla239b.pdf is named “How to Configure DP838xx for Ethernet Compliance Testing”, so I guess that register initialization should be the same for DP83867 & DP83869?
Regards,
Sreenivasa