Other Parts Discussed in Thread: DS90UB947-Q1, DS90UB948-Q1
I'm looking for a SERDES solution that would enable the connection of a thermal camera with VoSPI. Any suggestions ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90UB947-Q1, DS90UB948-Q1
I'm looking for a SERDES solution that would enable the connection of a thermal camera with VoSPI. Any suggestions ?
Hello Jorge,
What speed of SPI do you need for this application?
Best Regards,
Casey
the frame rate is 9 frames a second, and the frames are 16-bit, 160*120 frames, so about 2.8Mbits/sec..
Hello Jorge,
My understanding is that the VoSPI device always acts as a SPI slave and the data is accessed by SPI reads from the master device.
I do not believe we have a solution in that case. We can support SPI passthrough with a combo of DS90UB947-Q1 + DS90UB948-Q1, but the max SPI read speed is based on the max back channel rate of these devices. With max BC speed, plus accounting for the sampling rate of the SPI block and the round trip delays, the max speed we can achieve for SPI read transactions through the SERDES link is 1.3Mbps.
I am not aware of any other TI solutions
Best Regards,
Casey