Part Number: DS90UB962-Q1
Hello team
I am reviewing datasheet of 962.
and I found some weird spec from datasheet and roadmap
1) roadmap shows " 962 doesn't support synchronous clocking mode.

but data sheet shows 962 can support synchronous mode

2) I understand 962 can support up to 3Gbps line rate from datasheet.

but REF clock range is 23~26MHz so that line rate would be 160XRef clock= over than 4Gbps.
this means this synchronous mode line rate 4Gbps is conflicted with 3Gbps spec.
and I also could see 4.16Gbps power data from 962 datasheet.

As I totally checked this device, this is same as 960 but this only has 1 CSI output port. Am I correct??
if so, this could work with 953 for 3.3Gbps CSI BW.
Could you pls help me understand 962 device functionality clearly??
Really thank for your support~
Thanks