Other Parts Discussed in Thread: LMH0318
Hello,
I must isolate the SDI signal on the PCB board. So my idea was to use a balun at the input. It should transform the unbalanced Signal from the BNC connector to an balanced signal, which I would connect to the IN+ and IN- of the LMH0324. Is this working? The datasheet only shows the use as an unbalanced input!
Vice versa, I also need to this on the output side with the LMH0318.
thanks and greetings
Matthias