Part Number: TVS0500
Hi teams
I have few questions about select a right TVS for eFuse protection circuit. Below is a simplify SBD of my system.
The output of eFuse will power the DC-DC which have 6V maximum voltage tolenrance.
The rated input voltage level is 5V. My question is:
- Should TSV0500 work for 5V power rail protection?
- The maximum Vclamp of TVS0500 is 9.2V base on datasheet, it will be much higher than DC-DC absorlute maximum voltage (6V). I understand this maximum voltage tolenrance is consitently DC value. I want to know how to make sure the short pulse of 9.2V transient voltage won't damage this device?