Part Number: TUSB8041
I'm working in a Production environment with a board design that calls for a TUSB4041. That IC can't be found due to the global chip shortage. Can the TUSB8041 be used as a drop-in replacement?
The pinouts appear to be the same. The design is USB 2.0 so it doesn't require SuperSpeed lines - those are all No Connected on the board design.
The only pins I'm not sure about are:
Pin 7 - this is SMBUSz on the 4041, and it's SMBUSz/SS_SUSPEND on the 8041. The pin is left floating in the board design. Will that cause a problem with the 8041?
Pin 8 - this is FULLPWRMGMTz/SMBA1 on the 4041, and it's FULLPWRMGMTz/SMBA1/SS_UP on the 8041. The pin is left floating in the board design. Will that cause a problem with the 8041?
Thank you.