Part Number: DS90UB941AS-Q1
Hi team
I would like to ask that:
In customer previous project, the mode of 941 is splitter, so their MODE_SEL0 is configured to pull up VDD_1V8.
However, in the current project, the application scenario for 941AS is not splitter mode. Since customer would like to use the same configuration of hardware and do not want to change the schematic (like a platform project) how could they be compatible with two different projects?
Could they also use MODE_SEL0 pulled up to VDD_1v8 in the current project? Will there be any problem or risks?
The current project needs to change the register configuration to switch the working mode right? Will there be any problem or risks?