This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65994QFNEVM: TPS65994EVM

Part Number: TPS65994QFNEVM
Other Parts Discussed in Thread: TPS65994AD

Hi,

   Can you please suggest what firmware is programmed to TIVA microcontroller on TPS65994EVM. I am not able to connect to the EVM using PC. Also let us know what firmware goes in to the TPS65994AD PD controller.

Can you please share these firmwares.

I am using application configuration tool 6.4.5

Regards,

Pramod

  • Pramod,

    Because of shifted time zones, I am going to give you a quick answer and then let others take over this response.

    The firmware that is released on all of our EVMs is a proprietary test firmware that we cannot release to customers. 

    The GUI is used to configure our base firmware patch for use in your system and it is released with the GUI, so you should have everything that you need to get started.

    In order to power and communicate with the EVM, you will need to provide the following:

    1. Ether a type C power connection by connecting a type C DFP (Charger) to either of the type C connectors or by connecting the Barrel Jack to a 19.5V Supply.  Many customers use a dell power supply for this purpose.
    2. a USB micro B connection to your PC.

    If you have made these two connections, then you should be able to connect the EVM to your PC for configuration by following the guide on the product page.