Part Number: DS90UB921-Q1
Dear TI Team:
I'm trying to use the internal test pattern generator to test the connection between DS90UB921 and DS90UB928(as follow).
The Display only supports 44MHz, 1152x576@60fps.

I try to test pattern from ds90ub921, but it can't display.
1. My test code is follow. Is it any wrong? or can I test pattern from ds90ub928?
i2cset -f -y 16 0x0c 0x66 0x03
i2cset -f -y 16 0x0c 0x67 0x05
i2cset -f -y 16 0x0c 0x66 0x07
i2cset -f -y 16 0x0c 0x67 0x80
i2cset -f -y 16 0x0c 0x66 0x08
i2cset -f -y 16 0x0c 0x67 0x04
i2cset -f -y 16 0x0c 0x66 0x09
i2cset -f -y 16 0x0c 0x67 0x24
i2cset -f -y 16 0x0c 0x66 0x04
i2cset -f -y 16 0x0c 0x67 0x80
i2cset -f -y 16 0x0c 0x66 0x05
i2cset -f -y 16 0x0c 0x67 0x04
i2cset -f -y 16 0x0c 0x66 0x06
i2cset -f -y 16 0x0c 0x67 0x24
i2cset -f -y 16 0x0c 0x66 0x0C
i2cset -f -y 16 0x0c 0x67 0x20
i2cset -f -y 16 0x0c 0x66 0x0D
i2cset -f -y 16 0x0c 0x67 0x06
i2cset -f -y 16 0x0c 0x66 0x0A
i2cset -f -y 16 0x0c 0x67 0x08
i2cset -f -y 16 0x0c 0x66 0x0B
i2cset -f -y 16 0x0c 0x67 0x08
i2cset -f -y 16 0x0c 0x66 0x0E
i2cset -f -y 16 0x0c 0x67 0x03
i2cset -f -y 16 0x0c 0x65 0x03
i2cset -f -y 16 0x0c 0x64 0x11
2. Refer to Exploring the Int Test Pattern Generation Feature of FPD[1]Link III IVI Devices.pdf, Table 3-9. Pattern Generator Clock Divider N Configuration (PGCDC1),
clock = 200Mhz / N
How to set 44Mhz ?
Thanks.