Part Number: TCAN4550
Hi Team,
Good day. I'm posting this for our customer and they are using TCAN4550 demo program.
Main concern of the customer is they cannot transfer messages with this IC. They are using the TCAN4550 demo program, and have updated the SPI abstraction layer as mentioned in the TCAN45xx Software User's Guide.
None of the functions called from the Init_CAN function return false, we can assume that they have configured the SPI abstraction layer correctly. However, when running the CAN_Test function, there is no no messages being transceived on the CAN_HI or CAN_LO pins while using a logic analyzer. The TCAN4550 connected to another microcontroller which is waiting to receive CAN messages - it is not seeing the messages either.
Could you please help us what we are missing here.
Thank you for your support.
Best regards,
Jonathan