This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: If we only use D0-D3 of 947 and output dual link, can 947 support 1920*1080*60?

Part Number: DS90UB947-Q1

Hi team,

As the title, if we only use D0-D3 of 947 and output dual link, can 947 support 1920*1080*60?

Thanks!

Jiawei

  • Hello Jiawei,

    Yes, this is supported but please note that in single OLDI mode the interface will be running at 2x the speed which means that the input jitter/skew requirements will be 2x tighter compared to dual OLDI. 947 already has strict OLDI input TIJIT requirements so the customer must take caution to ensure that the source can meet the input tolerance of 947

    Best Regards,

    Casey