When DS90UB941AS-Q1 is connected to two remote deserializers in splitter or independent mode which have the same physical I2C address, how can they be accessed independently via I2C?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When DS90UB941AS-Q1 is connected to two remote deserializers in splitter or independent mode which have the same physical I2C address, how can they be accessed independently via I2C?

Since DS90UB941AS-Q1 does not have port-specific I2C aliasing for the remote deserializer address, an override of the physical address for the port 0 deserializer is required.
Step by Step:
1. Set 0x1E = 0x01 on 941AS to select port 0
2. Set 0x03 = 0x9A on the 941AS to enable I2C passthrough
3. Set 0x00 = "Override Address" on the DES to assign the DES on port 0 to a different physical I2C address. Make sure that bit 0 of the register is set to 1 in order to enable register override of the strapped I2C address
4. Set 0x1E = 0x02 on the 941AS to select port 1
5. Set 0x03 = 0x9A to enable I2C passthrough
6. Set 0x01 = 0x01 or 0x03 to return PORT_SEL to default value
Now the DES on port 1 can be accessed with the default strapped I2C address and the DES on port 0 can be accessed with the "Override Address"
Best Regards,
Casey