Part Number: TPS65982-EVM
Hello, I'm using a TPS65982-EVM to evaluate a 30W PD USB charger using these negotiated levels of voltage:20,15,12,9,5V
The PC-TPS board communications is enstablished via I2C using a I2C/RS232 adapter and all 5 PDO voltage levels are well negotiated (as I see on Vbus).
I want to use an external DC load to evaluate the system current but I don't know where it can be connected to the TI board. For this application I'm using the dp switch configuration n.7 so the external FET path is active.
Is it right to connect the DC load to J6 pin 1?
Thank you
Carlo Pasetto