Other Parts Discussed in Thread: TLIN10283-Q1, TLIN10285-Q1
Hi Team,
I want to confirm about the possibility to use lower voltage for VSUP.
This is just confirmation to use LIN Transceiver.
For example, TLIN1028 is possible to use around 5.5V for VSUP.
However, it is lower than the voltage of LIN Bus line.
If LIN Bus line is using around 12V, the device: TLIN1028 is possible to use on around 5.5V for VSUP?
Because some of internal circuit is operating on VSUP, but the input voltage is according to LIN Bus.
Therefore, I am warrying about the leakage the current to VSUP from LIN Bus.
Also, it may make some damage to the device, I concern.
Could you give me the usage in the lower voltage for VSUP about the LIN transceiver.
Regards,
Toru