Part Number: DP83822I
Hello team,
When the input voltage to the reset pin is around 1V, COL changes from H to L. Does this mean that it is undefined between 0.8 and 1.7V?
*VDDIO is used at 3.3V.

Attached a waveform.

-Vertical
1ms/div
-horizontal
Blue line: DP83822I _RESET_N_18pin(500mV/div)
Purple line: DP83822I _COL_29pin(1V/div)
Regards,
Masa