Part Number: DS90UB960-Q1
Hi Team,
What is the recommended duration to run the BIST?
Thanks
Reed
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Reed,
I would recommend to set this based on your desired BER confidence level and the desired BER level you are targeting for your application. You can use a basic calculator like this to find the time: https://www.sitime.com/ber-confidence-level-calculator
The typical BER confidence level most designers use is >95%
For example if you test for 10 seconds you could have 98% confidence level of 1e-10 BER:

If you want >95% confidence level of 1e-12 BER then you would need to run for ~15mins:

Best Regards,
Casey