Other Parts Discussed in Thread: ONET8501P, ONET1151P, ONET1151L
Team,
Could you please help with the below question:
For this project we want to amplify the signal delivered from an external fast photodiode amplifier of a third-party company via coaxial cable (bandwidth up to 10 GHz) so that it can be processed by a fast frequency divider .
We came across TI's "Optical networking ICs", for example the ONET1191P and ONET8501P. but have no experience with such devices.
We saw there are no EVM boards for these components so we designed our own PCB for evaluation (see pics attached) but we have issues the board.
The two boards with the ONET1191P show the following behavior:
"When the input is not terminated, the amplifier becomes an oscillator, and this is consistent with both PCBs.
This oscillating output frequency is typically around 6GHz and can be considered (at least in the two board we designed) as an "independent LO-level" in normal operation. This means that an input signals with lower levels (<-20dBm) and higher frequencies (>1GHz) (can) generate new output frequencies that are at n*F(e) +/- m*F(LO), thus appearing as a kind of "multimirror".
If signals above approx. 6GHz are applied to the input, no signal at all appears at the output that can be directly derived from the input, but only mixed signals from the upper sideband, and even the input level plays only an insignificant role.
This oscillating behavior can be influenced (if necessary) by putting a shield over the component - the undesired circuit behaviour may be reduced, or perhaps just shifted in the frequency products, or even underlined."
So the circuit does not seem to behave as we think it should.
I will provide picture of the boards offline as well as a block diagram of what we want to achieve in this project.
-Does this behavior sound familiar?
-Are there some ready to use EVM for ONET1191P and ONET8501P that can be used for evaluation?
-Could you provide feedback about the board/PCB we designed?
-Do we have some PCB guidelines, reference designs and even tips for the board design (like placement and type of connectors,..etc)
Thanks in advance,
A.