Part Number: TCA5405
Hi Team,
The TCA5405 datasheet doesn't seem to specify timing requirements for the pins in terms of power supply. Should VCC be provided before high level on DIN occurs? Our customer noticed that sometimes outputs are high for a short period of time during power on scenario of the final system with the master host that manages the IC.
They did performed a simple experiment: They provided high level to DIN from external power supply 1.8V and triggered VCC (1.8V too) few times. In almost all of the time, inputs become high on power on. In most cases they remain high. It looks like there is a requirement not to have a high level on DIN before the IC is fully powered exist.
Unfortunately we can't locate a timing/sequencing requirement in the datasheet. Can you help us specify these requirements precisely to our customer? Thanks in advance!
Kind Regards,
Jejomar