Other Parts Discussed in Thread: SN65HVD21
Interface team,
I have a customer exploring different options to maximize the # of nodes, length, and speed of a 485 line. Can you help to answer their questions below?
1) I’ve been looking at available RS485 transceivers and realize that there may not be a part that meets all of the requirements. It looks like the SN65HVD21 may be a good compromise, with us operating around 100 to 255 nodes across 255 feet of cable at 5Mbps. We may be able to lower our supply voltage to less than the 27V max rating of the part. Are there any other suggetions?
2) Do you think we will be able to obtain 5Mbps over 255 feet of cable when connecting that many nodes along the bus? My concern is the input capacitance of each transceiver on the bus degrading the signal. Our system architecture may only need one receiver enabled at any given time using a TDMA approach, so we can disable the rest of the receivers on the bus.
3) Would disabling the driver and receiver on the RS485 transceiver reduce the differential capacitance that the bus is exposed to?
Thanks,
Tom