Hi TI Ethernet IC Engineers,
We are using retimer DS250DF810 in our ICX-7650 platform for 100G port.
Switch side, it is connected to TSCF2 of BROADCOM BCM560568.
When Broadcom 100G BiDi QSFP optics [AFBR-89BDDZ] inserted into 100G port, there is no signal in the detected at peer side.
When SR4 QSFP optics inserted, it works fine.
With register dump, we observed no signal detect and CDR lock at the line side.
Here are dump of shared registers.
ICX7650-48ZP Router#dm i2c-read 7 18 00 <-- read register at address 0x00
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 01 <-- read register at address 0x01
0x30
ICX7650-48ZP Router#dm i2c-read 7 18 02
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 03
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 04
0x9
ICX7650-48ZP Router#dm i2c-read 7 18 3d
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 3e
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 3f
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 0a
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 10
0xff
ICX7650-48ZP Router#dm i2c-read 7 18 05
0x1
ICX7650-48ZP Router#dm i2c-read 7 18 06
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 07
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 08
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 09
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 0b
0x40
ICX7650-48ZP Router#dm i2c-read 7 18 0c
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 0d
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 0e
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 0f
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 10
0xff
ICX7650-48ZP Router#dm i2c-read 7 18 11
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 12
0x91
ICX7650-48ZP Router#dm i2c-read 7 18 13
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 14
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 15
0x0
ICX7650-48ZP Router#dm i2c-read 7 18 16
0x0
ICX7650-48ZP Router#
We use following channel settings for all 8 channels
- FIR Main Cursor register:-
register address = 0x3D
Register value = 0x19
- FIR Pre-Cursor register:-
register address = 0x3E
Register value = 0x04
- FIR Post-Cursor register:-
register address = 0x3F
Register value = 0x01
Kindly help to make link up through re-timer DS250DF810.
Thanks,
Prabhat