Part Number: DP83TC812S-Q1
Hello,
For reliability and redundancy purposes, and for very small overall network length (<1m), we would like to switch the TRM lines between 2 targets.
We would then like to know the output common mode voltage of the TRD pins, or at least a value of the minimum and maximum voltage for the two differential pins. If that is not known, we would have to DC-block and re-bias in an additional stage, which is not desirable. Having this data with different VDDIO possible values would be even better.
Thank you.