Part Number: TS3DV642
I have a question regarding the SCL/SDA/HPD/CEC pins on the TS3DV 642.
・Is it OK to input the LVDS signal to the SCL/SDA/HPD/CEC pin?

・What are the Tskew characteristics of the SCL/SDA/HPD/CEC pin?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS3DV642
I have a question regarding the SCL/SDA/HPD/CEC pins on the TS3DV 642.
・Is it OK to input the LVDS signal to the SCL/SDA/HPD/CEC pin?

・What are the Tskew characteristics of the SCL/SDA/HPD/CEC pin?

Hi,
Yes, you could I use SCL_A_B / SDA _A_B and HPD_A_B / CEC_A_B signal paths on the TS3DV642 as general purpose LVDS signal switching. These paths are not different than the other signal paths in the device but are labeled differently to match up with the signals used in HDMI applications.
So the skew in the datasheet will apply toward these signals as well.
Thanks
David
Thank you. This resolved my issue.