Part Number: DS90LV011A
Hello team,
I received a question from the customer.
Application note slla014a advises to set the characteristic impedance to 90 to 130 ohms, is it the range in the red box that should be 90 to 130 ohms? Or is the range including the range from the cable to the receiver(BLue)? Also, in the case of the red frame, is it necessary to set the characteristic impedance to 90 to 130 ohms on the transmit and receive sides, respectively?

Regards,
Masa