Hi,
For multiple I2C switches, somebody mentioned that we need to keep an eye on ViL of I2C if we have multiple switches in the path. I was confused with the answer because only one device is able to answer to master which means that only one slave device will be asserted low when it talks to master. Why should we worry about the current limitation on I2C line when its low. Can you please clarify. I want to use three I2C switches in series with two of the switches connected to multiple slave devices on their respective downstream channels as shown below. Do I need to worry about any thing like overall capacitance and driver strength etc in below circuit diagram. FYi the third switch is just to isolate another master.
Regards
Owais