Part Number: TUSB1142
hi,
i am using the tusb1142 part to drive a usb C 24 pin connector. I am running usb 3.2 gen 2.
I will be driving a cable up to 6 feet long. is there a default pin config that you would suggest for my prototype design?
thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB1142
hi,
i am using the tusb1142 part to drive a usb C 24 pin connector. I am running usb 3.2 gen 2.
I will be driving a cable up to 6 feet long. is there a default pin config that you would suggest for my prototype design?
thanks,
Hi,
How much is the loss of this 6ft cable? The max insertion loss for the cable for USB3.2 Gen 2 10Gbps is 6dB which is around 1m in length. Does this cable have better loss that the 6dB?
Thanks
David
No idea what the end user cable length or loss will be. I was hoping to use the PIN config function of the TUSB1142 part. Is there a pin config that works best in most cable scenarios? I am connecting the TUSB1142 between my USB3.2 HUB and a USB-C connector.
thanks
Hi,
Please see this simplified block diagram for reference,

TUSB1142 can only provide linear re-driver function on the TX path, it does not have TX SWING or Pre-/De-emphasis to compensate for the cable loss. So the compensation for the cable loss has to come from the hub itself. But a USB3.2 compliant hub will only work with a cable that has 6dB loss at 10Gbps as defined by the USB spec. If the cable loss is outside the -6dB loss, then the data rate will drop from 10G to 5G.
Thanks
David
David,
thank you for the reply,
This is the first USB 3.2 and USB-C project i have ever worked on. Gaining knowledge as fast as i can.
this is excellent information. Can you suggest a better part from TI to use? I considered the USB C switch only part , is there a better part for a USB 3.2 hub to USB-C offboard connector scenario?
Thanks,
Hi,
TUSB1142 or the TUSB1042 is the right part for this design. Refer to this loss budget white paper from USB.org, https://www.usb.org/sites/default/files/USB_3.1_Loss_Budget_Rev_1.0_-_2015-03-02.pdf, you can only drive a passive 6dB cable with 10Gbps (Gen 2). Most likely the data rate will drop to 5Gbps (Gen 1) when driving the 3m cable.
Thanks
David