This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1002A: AC coupling capacitor for SATA only

Part Number: TUSB1002A

Hi,

I'd like to confirm the value of AC coupling cap for SATA only application.
Ii is clear to have the ferrite bead along with 49.9 ohm resistor at between C(TX2) and SATA connector.

For AC coupling capacitor, there are 10nF nearby intel chipset SATA TX and RX already.
- Does it still need all TX1, TX2, RX1, and RX2 A/C coupling capacitors?
- If so, the value is as below, right?
  TX1, TX2, and RX2 A/C coupling capacitor : 220nF
  RX1 A/C coupling capacitor : 330nF

Thanks
Mark