This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

It is common for an Ethernet PHY to support multiple speeds, e.g. 10/100/1000Mbps. For various use cases, it is desired to operate at a single speed. There are two main ways to do this that are discussed below:
It is important to note that for both options, Auto-neg and Forced, both parties of the link chain need to be in the same mode. I.e. one PHY with Auto-Neg enabled and the other with Forced Speed will NOT link up. Both need to be Auto-neg or both Forced. Please refer to the table 1 below.
Table 1- Auto-neg/Forced Speed Set up
|
DUT |
Link Partner |
Link up/ No link up |
|
Auto negotiation |
Auto negotiation |
Link up |
|
Force mode 100mbps |
Force mode 100mbps |
Link up |
|
Auto negotiation |
Force mode 100mbps |
No link up |
Note:
Regards,
Hillman Lin,
Alvaro Reyes