Part Number: TPD4E02B04
Other Parts Discussed in Thread: TPD4S009, TPD2E001
Please help suggest if TI has similar products?
1. ECMF02-4CMX8 STMICRO
2. HSP062-2M6 STMICRO
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In regards to the ECMF02-4CMX8 STMICRO, we don't have any ESD devices with an integrated common mode filter. A comparison table including HSP062-2M6 and TI recommendations are shown below:
| HSP062-2M6 | TPD4S009 | TPD2E001 | |
| Vrwm (V) | 24 | 5.5 | 5.5 |
| Package Type | uQFN | USON | USON |
| Package Size (L x W) (mm) | 1.45 x 1 | 1.45 x 1 | 1.45 x 1 |
| Polarity | Unidirectional | Unidirectional | Unidirectional |
| Number of Channels | 2 | 4 | 2 |
| Clamping Voltage | 18 | 20 | 16 |
| IO Capacitance (typ) (pF) | 0.6 | 0.8 | 1.5 |
| IEC 61000-4-5 (A) | 3 | 2.5 | --- |
| IEC 61000-4-2 Contact (kV) | 8 | 8 | 8 |
Please let me know if you have additional questions.
Best Regards,
McKenzie Eaker