Hi, TEAM.
Could you please continue to support the thread below?
e2e.ti.com/.../4843374 4843374
a. Please tell me the mechanism of thermal shutdown.
It seems that the IC does not have a thermocouple inside to detect it, so isn't overcurrent detection or overvoltage detection detected as thermal shutdown?
b. Once inside the company, we were unable to measure the temperature when the TXDB was not outputting (the same phenomenon as at the site was reproduced), and we have not repeated it since then.
However, when we assembled the same configuration and measured the temperature, the surface temperature of the parts was around 43°C.
I think it's hard to imagine a thermal shutdown at around 43℃,
Is it possible that the same event (such as thermal shutdown) could occur in other cases?
c. Also, is it possible that the manufacturing process of the SN751178NS has made thermal shutdown more likely to occur (for example, the surface of the package has become thinner)?
Although it has been changing the circuit, it did not occur in the old lot.
Thank you.