Part Number: DP83849I
HI
PWRDOWN_INT_A should float/suspend, but the default function for this pin is POWER DOWN. Is there a problem with the use of device functions at this time?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83849I
HI
PWRDOWN_INT_A should float/suspend, but the default function for this pin is POWER DOWN. Is there a problem with the use of device functions at this time?
Thanks
Hi Shitong,
The PWDDOWN_INT_A (Pin 18) functions as POWER DOWN by default. It has an internal pull up resistor and this pin is active-low. If this pin is going to be unused, it is okay to leave it floating. This will not cause a problem with the device.
Regards,
Alvaro