Part Number: DP83869HM
Hello All,
I am currently using 4 numbers of DP83869HM ICs in my design. 2 of which are having VDDIO as 3.3V and 2 of them are having VDDIO of 1.8V. These are connected as shown in the figure below
Now the ones connected to 3.3V are working fine. There are no data inconsistencies on them.
But the 1.8V ones are giving unstable data. While probing the "mii info" command from uboot of NXP processor, the vendor ID keeps on changing on every probe as shown below.

PHYs 0x0A and 0x0E are 3.3V PHYs and PHYs 0x0B and 0x0F are 1.8V PHYs. You can see the inconsistency in OUI and other details.
I have also attached the PDF with the schematic of the 1.8V PHYs. Please help with this.
Schematic of 1.8V DP83869 PHYs.pdf
Thanks and Regards,
Souvik