Part Number: DS90UB941AS-Q1
It is possible for two screens that is "sync mode" to have different sync polarity requirements,
how does the 941+ 948x2 handle this situation?
can 948 or 948 can revert POLARITY of only one port of FPD3 output?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
It is possible for two screens that is "sync mode" to have different sync polarity requirements,
how does the 941+ 948x2 handle this situation?
can 948 or 948 can revert POLARITY of only one port of FPD3 output?
Hi, just to clarify what are you referring to by "sync mode"? And when you mention polarity of FPD3 output, you are referring to the sync signals right? Or are you also looking to swap the polarity of the FPD-link traces? Because that would be a different case.
For asymmetric splitting are you using cropping and a single DSI input? I will check about whether hsync,vsync have to be same and get back to you by Thursday.
Best regards,
Ikram
I am refering to POLARITY of 948 output LVDS sync signal. both LCD pannel care about hs&vs signal. but they requst different hs&vs signal polarity.
i am using single DSI input and make croping.
Hi, I am looking into whether there is a way to swap the polarity with cropping and one DSI input. I will get back to you by Friday.
Best regards,
Ikram
Hi, with this device cannot support changing the polarity on one port with one DSI input and cropping.
If possible, you could consider having cropped video inputs to two DSI ports with different sync polarity and sending them on each FPD-link port (DSI0 to DOUT0, DSI1 to DOUT1), similar to Independent 2:2 Mode described in the datasheet.
Best regards,
Ikram