Part Number: DP83640
Hi,
I am working with the ATSAME70N21 combined with DP83640. My firmware is built with FreeRtos 10.0.0 and LWIP 2.1.2.
My goal is to implement a PTP slave with Ordinary Clock.
1) Is there a RTOS driver for DP83640? I only found a linux one for DP83640 and a RTOS only for DP83867.
2) I had a look at the library provided in https://www.ti.com/tool/DP83640SW-LIB.
Should I copy EPL to my project to use it to configure the DP83640 for PTP?
Is this library enough or is there an example/demo that I can check for configuring DP83640?
3) I see two options for the PTP application: PTPd and PTP4l, would you suggest one over the other for my case? I noticed that most of the examples I found online use PTPd, despite it is an older implementation.
4) Also, do you have any suggestion for an example/patch on the required changes for LWIP?