Part Number: SN65DSI84-Q1
Other Parts Discussed in Thread: DSI-TUNER
Hi team,
I have a question here that if screen can't display the normal picture. What information can be read from the register of this IC using I2C for debugging?
BR,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI84-Q1
Other Parts Discussed in Thread: DSI-TUNER
Hi team,
I have a question here that if screen can't display the normal picture. What information can be read from the register of this IC using I2C for debugging?
BR,
Jimmy
Hello, Jimmy,
There are a number of steps you can take to debug this type of issue.
1. First, verify that you are following the initialization sequence listed in the datasheet. This sequence is critical for correct operation of these devices. Below is an example of what the initialization sequence should look like on an oscilloscope:
2. Verify that the video timing output from your processor matches what you are programming into the DSI83/DSI84/DSI85. This includes the DSI CLK frequency, active pixel data, and blanking pixel data. Video input timing, register configuration, and the panel timing requirements all have to match up for the video streaming to work without errors.
3. Make sure the LVDS timing parameters are within specification of the display panel datasheet.
4. Make sure the line time (time from HSYNC to HSYNC) on the DSI input matches the line time on the LVDS output. The line time on the LVDS output is the total amount of horizontal pixels divided by the LVDS clock frequency. You can measure the line time on the DSI input with an oscilloscope by zooming in on the data stream on of the data lanes like below:
The easiest way to configure these devices is to use the DSI-Tuner tool. You can reference these training videos to quickly understand how to use it for your application:
The DSI-Tuner will allow you to configure most of the device registers without having to look through the register map, and will provide feedback on whether or not the line time requirement has been met.
Thanks,
Zach