Part Number: TCA9548A-Q1
TCA9548ARGERQ1
Hi,
I have been using TCA9548ARGERQ1 I2C Switch in couple of our projects. I need help for two issues facing in I2C which are mentioned below,
i) I found that even though no load is connected to TCA9548ARGERQ1 I2C Switch. For I2C SCL & SDA, VOL (Low Voltage Level) not maintained at 0V.
I have checked with different pullup resistor values (1k, 1.5k, 4.7K & 10K) but could not be able to reduce the VOL value to "0", it is maintained at 200mV for 4.7K Pullup. Please find the reference image below.

I could not be able to find original reference images in TCA9548ARGERQ1 datasheet.
It is in the range of recommended working voltage of the device (Max. VOL value supported is 0.3*1.8 = 0.54V), but we want to reduce that voltage to "0V"?
Kindly let me know why it is happening like this and recommendations to avoid such issues.
ii) One more issue is when connected with the load, there is toggle in low voltage level as shown in figure below. Device is working fine in below situation too.
But I need to solve this issue. In this case also we checked the issue with different resistor values like 33Ohms (not working), 1K, 1.5K, 4.7K, 10K and 105K. In all above cases same behavior is maintained.
Please help me with this issue.

Thanks,One more issueii22fc
Sampath Burra.