This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Regarding unused pins, the following answer was given.
No; these logic inputs must not be allowed to float, so you need to connect them to VCC or GND.
7.3.2 of the datasheet states that there is a pull-up resistor.
I hear that there is a pull-up resistor, but is it better not to use it open?
Hi Shinji,
I need to verify if the TIN pins have an internal pull up resistor. Since I do not see a functional block diagram of the device with internal pull up resistors in the diagram, I'm a little hesitant to confirm they actually exist. Sometimes datasheet errors are carried over from previous datasheets or have errors that were never caught.
If TIN has internal pull up resistors then you can leave them floating. If they do not, then you must reference the pins to either GND or Vcc.
I'm currently checking to see if I can find a design engineer who can confirm TIN has internal pull up resistors, I will get back to you when I find out.
Sorry for the delay,
-Bobby