This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: Listen only mode

Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550

Hello ,

We are using TCAN4550 driver, is this driver supports listen only mode for auto baudrate feautre?

  • Hello Tanushree,

    Yes, the setting the MON bit in the Control register 0x1018[5] to "1" will disable the driver and enable the Bus Monitoring Mode which is essentially a "listen only mode".

    There is not an Auto Baudrate feature, but you would need to determine that through an iterative bit timing configuration of the device to determine when the received data was correct.

    Regards,

    Jonathan