Dear all,
if TUSB73x0 superspeed interfaces(such as USB_SSRXN_DN2/SSRXP_DN2, USB_SSTXN_DN2/TXP_DN2 ) are NOT used, can they be floating directly? thanks.
best regards,
Steven
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
if TUSB73x0 superspeed interfaces(such as USB_SSRXN_DN2/SSRXP_DN2, USB_SSTXN_DN2/TXP_DN2 ) are NOT used, can they be floating directly? thanks.
best regards,
Steven
Hello,
Yes, Unused USB 3.0 terminals must be left unconnected, terminating unused USB 3.0 signals is not recommended.
Regards.